Returns the first operand that is not equal to NULL. If all operands are NULL then returns NULL
Format
COALESCE( Operand1, Operand2 [, Operand]* )
Remarks
This is a shorthand form of the CASE statement.
The expression:
COALESCE(x,y)
is equivalent to:
CASE WHEN x IS NOT NULL THEN x ELSE y END
The return value is the first nonnull operand or NULL if all operands are equal to NULL.
Operand1, Operand2 and Operandcan be any expression.
COALESCE( CurrentStateDesc, 'Unknown State' )